Home Online Store Products Literature My Omega Omega Info Contact us View Cart Help Global
search
         
 
Two-Wire Transmitters
For Temperature Applications

( Printable Version )

A two-wire transmitter is an ideal solution for many remote temperature measurement applications. Transmitters have definite advantages over conventional temperature measuring devices, but must be selected with caution in order to avoid “ground loop” problems.

PURPOSE
In many cases, the temperature of a remote process must be monitored. Common temperature sensing devices such as thermocouples and RTD’s produce very small “signals.” These sensors can be connected to a two-wire transmitter that will amplify and condition the small signal. Once conditioned to a usable level, this signal can be transmitted through ordinary copper wire and used to drive other equipment such as meters, dataloggers, chart recorders, computers or controllers.

OPERATION
A two-wire transmitter draws current from a remote dc power supply in proportion to its sensor input. The actual signal is transmitted as a change in the power supply current.

Specifically, a thermocouple input transmitter will draw 4 mA of current from a dc power supply when measuring the lowest temperature of the process. Then, as the temperature rises, the two-wire transmitter will draw proportionally more current, until it reaches 20 mA. This 20 mA signal corresponds to the thermocouple’s highest sensed temperature. The transmitter’s internal signal-conditioning circuitry (powered by a portion of the 4-20 mA current) determines the temperature range that the output current signal will represent.

Physically, only two copper wires are necessary to connect the transmitter output signal in a series circuit with the remote power supply and the process equipment. This is made possible since the signal and the power supply line are combined (one circuit serves a dual function).

ADVANTAGES
Two-wire transmitters offer numerous advantages over the more traditional ways of measuring temperature.

1.ac power is not needed at the remote location to operate a twowire transmitter.
Since transmitters are powered by a low level 4-20 mA output current signal, no additional power has to be supplied at the remote location. In addition, the usual 24 Vdc signal necessary for operation is standard in plants that have large amounts of instrumentation.

2.Electrical noise and signal degradation are not a problem for two-wire transmitter users.
The transmitter's current output signal lends itself to a high immunity when it comes to ambient electrical noise. Any noise that does appear in the output current is usually eliminated by the common-mode rejection of the receiving device. In addition, the current output signal will not change (diminish) with distance as most voltage signals do.

3.Wire costs drop significantly when using two-wire transmitters.
Low voltage signals produced by thermocouples almost always require the use of shielded cable when they are sent any significant distance. Ambient electrical noise from arcing electrical relays, motors and ac power lines can raise havoc with these signals that are transmitted in an unshielded cable. In addition, expensive, heavy gage wire is often installed in applications that call for long cable runs (since it reduces errors from signal voltage drops caused by line resistance).

Ordinary copper wire can be used to connect all the pertinent equipment in a two-wire transmitter system. The 4-20 mA current output signal is relatively immune to ambient electrical noise and is not degraded by long distance transmission, even over a small diameter wire. Adding a two-wire transmitter to a system eliminates the problem of having to provide long runs of costly wire and an extensive amount of shielding.

GROUND LOOP PROBLEMS
If a grounding rod was driven into the earth at two different points and a voltmeter was connected between them, a voltage difference would be detected between the two. This difference in potential exists between practically any two points along the earth’s surface. When one tries to measure a process that is at a remote location, this voltage difference will induce an error current along the line, which is referred to as a “ground loop” signal. Its result will be an error at the display.

To prevent “ground loop” errors of this type, select an isolating two-wire transmitter for your system. This type of transmitter will optoelectronically isolate the sensor signal from the output current loop. This will allow the user to ground both the sensor and one side of the current loop.

TRANSMITTER FEATURES
Transmitters provide a two-wire output with the same wiring used for power and output. The load resistance is connected in series with a dc power supply, and the current drawn from the supply is a 4-20 mA or output signal which is proportional to the input signal.

Two-wire transmission permits remote mounting of the transmitter near the sensor to minimize the effects of noise and signal degradation to which low level sensor outputs are susceptible.

A rugged metal enclosure, suitable for field mounting, offers environmental protection and screw terminal input and output connections. This enclosure may be either surface or standard relay track mounted.

Most two-wire transmitters are linearized to the voltage signal produced by the thermocouple or RTD, although there are new models now available that are linearized to the actual temperature.

The two-wire transmitters convert the thermocouple or RTD signal to a 4-20 mA output signal. Some models will convert to an RS-232C output. Transmitters are available with dip switch selection for several thermocouple types per model, as well as thermocouple and RTD selection on a single model. Two-wire transmitters are available in either isolating or non-isolating models, and they also feature output ranging adjustments with zero and span adjustments over 80 to 100% (depending on model) of the sensor range.

© Copyright 2003-2025  |  OMEGA ENGINEERING, Inc. | OMEGA Privacy Statement